Other Parts Discussed in Thread: TAS3251, , TAS3251EVM
I am beginning work on a system with a 2.1 configuration. I am considering the following: stereo TAS5825M (BTL) for L and R and mono TAS3251 (PBTL) for the low frequency driver. I have some questions about how to support this using the PPC3 software.
Here are three scenarios I can see working and questions related to each:
- In the TAS5825M PPC3 module, there is a 2.1 configuration that supports the TAS5825M driving two tweeters in stereo mode operation. It also provides support for I2S connections to drive a non-Smart Amp device like the TAS5720/60. The support for a mono I2S feed to the non-smart amp is what I need, but I want to use the TAS3251 in this application.
-
- Is it possible to use this TAS5825M 2.1 Configuration – and also have a separate PPC3 tuning file that I use to configure the TAS3251?
- Is there a configuration I can use that supports these two TI Smart Amps in PPC3 with a single tuning file? This would greatly simplify the crossover tuning
- The TAS3251 PPC3 module supports a Mono, PBTL I2S input configuration. It looks like this can support all the tuning and Smart Amp features I need for my application
- Does this configuration require the TAS3251 to be configured as an I2S Slave device?
- The TAS5825M does not seem to have the feature where it can configure MCLK as an output to drive the input on the TAS3251. Is this correct?
- Ideally, this would be supported with a single PPC3 file for both amps.
- If separate PPC3 Speaker Characterization and Tuning files are required, can this be supported with a single I2S stream from a Bluetooth Sink device?
Also, regarding TAS5825M, I am in the process of developing my own EVM of sorts. Ideally, I would like to be able to perform tuning adjustments (like EQ and DRC) in real time on either device while listening to audio tuning files. Is this possible?