Part Number: PUREPATH-CMBEVM
Other Parts Discussed in Thread: TAS5756M, TAS5754MDCAEVM, TAS5756MDCAEVM
Hello,
I bought a PurePath Motherboard to program the DSP in the TAS5756M.
I have installed PurePath Console 1, PurePath Console 2 and PurePath Console 3.
With PurePath Console 1 and 3 I can connect to the motherboard without any problem.
I connected the TAS5756M board and with PurePath Console 1 I dump the Register of the TAS5756M.
I try to write something with the Command Buffer Interface and it works.
So the boards work.
With PurePath Console 2 I can't connect to the motherboard or with the TAS5756M.
If I click on "Connect asTAS5754M-56MDCAEVM" the device connects for less than a second and the unexpected FWID warning pop-up appears again.
Following this user guide: www.ti.com/.../slau583.pdf
at "3.5 Firmware ID Update" - I can't change the FWID because the FWID button in the Device Settings section of the Direct I2C Read/Write tab is greyed
I don't think the problem is in the wrong FWID, because the PurePath Console 1 and 3 work.
I tried to install the PurePath 2 in another computer and I have the same problem.
Please help me. I have the prototype on my desk and I have a few time to complete it.
The DSP configuration is the last thing to do.
Thanks.
Thank you in advance.
Best Regards,
Davy