Hi,
I have two TLV320AIC3254EVM boards, I was using them without any problem in the beginning, then I changed sampling rate from default 44.1kHz to 48kHz, it showed something like, the sampling rate is not aligned with EVB, firmware needs to be updated, and I clicked yes, everything went well (except it wants we to select board FWID, I didn't know what to select so I cancel it, but the GDE still worked), however after couple hours EVM unplugged, I could not connect it back! My windows 10 is always showing the USB is not recognized, AIC3254 CS also shows EVM disconnected.
I thought it was the first one went down because some hardware reasons, but It happened on my second boards! The second one ran well in the beginning as well, now it is malfunctioned like first one after I did the same things.
I saw a related question here, tried to re-install ESBEVM driver, however it keep showing "download failed" at step 6 following the instruction, what can I do now? It's urgent!
Thank you,
Pierce