Other Parts Discussed in Thread: TAS6424
Dear expert,
I see that datasheet listed the output power, this is based on sine wave before clippling, right?
4 Ω, PVDD = 14.4 V, THD+N = 1%, TC = 75°C 22W
My question is, if I further increase the volume, which increasing the output power by making output waveform clipping, what's the maximum power I can obtain?
I see there's only temperature preventing me from obtaining this maximum power. The over current limit won't prevent me because the peak current is same as before, right?
By the way, will PA be damaged this way?
Thank you.