Part Number: TAS5825-SW
Other Parts Discussed in Thread: TAS5825M
Hi!
My customer is building up the EQ Tuning in the customer system by using the PPC3 tool to output the EQ Tuning as a dump file.
However, the expected tuning sound is not being output.So the customer is reviewing each of the Register settings.
What is the difference between RAM mode and ROM mode in the figure below regarding the 0x40 register?
Can you tell me the difference between the modes below and the exact definition of the modes below? The Datasheet does not provide details.
1.RAM MODE
2.ROM MODE1
3.ROM MODE2
4.ROM MODE3
If 0x40 register is set to 0x00, the desired sound is outputted to 0x10, without the desired sound being output.
In addition, how do we set the test values in the EVM in a dump file so that we can build up our system?
There are five dump modes. Can you tell me the exact definition of the menu below?
1.default
2.current state
3.snapshot
4.current state -cold boot
5.custom
Please check it.
Thank you.
Best Regards.
From Anthony.