Other Parts Discussed in Thread: DIR1703
Hey team,
The datasheet says to connect a 24.576 MHz resonator to the DIR9001, as shown below.
I was wondering if I could use a 12.288 MHz crystal and connect it as shown below. Will it still work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
No, a 12.288MHz XTAL will not work w/ the DIR9001. This is covered in Table 1 in the datasheet which discusses the differences between the DIR1703 and DIR9001. As noted in the table, the DIR9001 only supports a 24.576MHz XTI inputs.