This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: How to configure the input of OSC_M and OSC_P of TPA3255 in slave mode

Part Number: TPA3255


Dear team,

I need to use a low frequency of PWM frequency like 50kHz to my TPA3255, so I need to configure TPA3255 as slave mode, then use an external clock source connect to OSC_M and OSC_P.

Q1: Can you tell me how to configure external clock source that connect to  OSC_M and OSC_P ?

Q2: Can I use a 50kHz external square connect to OSC_M and OSC_P?

Q3: What's the requirement of the external clock that connect to OSC_N and OSC_P?

Thank you!

Best regards