Dear all
I'm observing HPOUTs voltage at power up (causing audible pop), HP outs are used in single ended mode; connected to the headphones connector through 47uF electrolytic caps.
HPCOMs are left unconnected.
My power up sequence is as follow :
1- Keep reset pin low
2- Start power supply 3.3V digital IOVDD
3- Start power supply 3.3V analog + 1.8V Digital (DRVDD+AVDD+DVDD)
4- Wait about 30ms then Start I2S clocks
5- Wait about 5ms then Set reset pin high
6- Wait about 5ms then Configure codec registers
I'm observing a voltage ramp up on HPOuts about 5 to 6ms after step 3; once the analog power supply is provided.
By default all HPOut amps should be powered off, I do not understand why I observe those voltage on HPOUTs pins ?
Any idea would be greatly appreciated.
Thanks.