This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1860: State of INT w/o sys. controller

Part Number: PCM1860

I have a new design that does not have a microcontroller connected to INT (PIN 19), like example shown in section 10.2 of the datasheet. Can TI confirm that this pin can be left floating?

  • Hello,

    It is recommended to place a 10k pull-down to GND on this pin instead of leaving it floating.  If it's driven high due to an external ESD or transient event while left floating then the PCM1860 would be placed in a powered-down (idle) state.

  • Per datasheet page 9, pin functions table, Pin 19 states "Pull high for active mode, pull low for idle.". Doesn't this contradict what you are saying here? Which statement is correct?

  • Hi Steven,

    The discrepancy in the page 9 pin function table is a known error in the PCM1860 datasheet and will get updated during the next revision.  The applications sections and PCM1860 power-down  information (pages 60 and 76) describes the correct operation which is driven high for idle (mute) mode and driven low for active mode.  We have tested this behavior on an EVM and have confirmed it in the past.