the communication via I2C to PCM5121 is working, with SCLK=24.576MHz and BCLK=12.288MHz, Sample Rate is 48kHz.
There are 8 TDM Slots with 32-Bit Samples (the other 6 Slots are used by three TAS 6422, which are working well.)
The PCM5121 is configured accordingly, while using its Auto Clock function. BUT, the PCM5121 does stay in the mode of 'Volume Up Ramp' and so keeps to be muted. (Register 0x76 shows the value 0x84) - Do you know why and how to solve this issue?
The customer tried to switch from active to standby and back again, but PSM5121 stays muted.
Thanks for your support!
ciao
Hanno