Hi,
I making a project for school and am using the PCM1802. I connected it and it works normal when I put something on the input (Analog output). Right now I want to see the difference when I set THE BYPAS on HIGH to see the DC on the output. Unfortunately It does not work ( it still only shows only the ANALOG). I even connected 2V to the input to have a pure DC input and it showed nothing on the DOUT. What can be the cause of that? Can it be solved?
Thank you in advance,
Filip