This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 191
Part Number: LMV1012
Hi Sir,
My customer is currently using MAX4063A, we would like to replace it and found that LMV1012 looks similar to it. But I am not familiar with Microphone Preamplifier, could you help check if we have a good solution to replace it?
Many thanks,
Patrick
Hi Patrick,
Do you have a data sheet of the competitor device?
LMV1012 is the kind of pre-amp that is used inside of the electret case. Is that what customer is looking for?
Best regards,-Ivan SalazarApplications Engineer - Low Power Audio & Actuators
In reply to Ivan Salazar:
Hi Ivan,
The spec link as below.
https://datasheets.maximintegrated.com/en/ds/MAX4063.pdf
Thanks.
In reply to Patrick Chen(TPE System & Application):
Patrick,
If customer only needs the microphone amplifier portion, then LMV1012 should be OK. There are several op-amps available as well if the package is too small to handle.
Unfortunately there is no direct part-to-part replacement for the mentioned device.