Part Number: TAS5825M
I have an application , that I need to be able to adjust EQ parameters on the fly through software. .This is something I have done many times before with the SigmaStudio processors Anyhow, I captured the I2S output from PurePath for a 48Khz peaking, filter Freq=1000, Q=.71, Gain = 12dB.which generates a I2S address, sub address and a series of 5 32 bit numbers in hex.. However, nowhere in the documentation is there an indication the coefficient load order and the actual coefficients don't seem to make sense. I understand that your implementation of Direct Form 1 has a 2x gain for B! and A1.
Do you have any additional information of time?