Part Number: TPA3255
Other Parts Discussed in Thread: PCM5121, , PCM5242
Hi,
we are using a PCM5121 DAC (2Vrms max output) and a TPS3255 in BTL mode.
When I output 2Vrms from the DAC and have 21.5dB Gain, I get ~24Vrms output voltage which results in 144W into 4 Ohms (this is also what I can measure).
But how can I reach higher output power - the TPA3255 product page says "The device is operated in AD-mode, and can drive up to 2 x 315 W into 4-Ω load at 10% THD and 2 x 150 W unclipped into 8-Ω load and features a 2 VRMS analog input interface" but how does this work then ?
And using our setup, I can only achieve ~145W output power without clipping ?
Is there a gain setting I have to do ?
And does the TPA3255 change it's internal gain depending on the SE / BTL / PBTL mode ?
Or do I need a buffer op amp to reach higher output power e.g. in PBTL mode ?
Regards,
Sebastian