Hello Steve
We have one query, actually we are are using a headset with this chip that has the following specs:
Speaker Specification | |
Type | Transducer Moving coil dynamic speaker |
Impedance | 1000Ω±15% @1KHZ |
Sensitivity | 115dB±10 at 1K |
Frequency respond | 200-4KHZ |
Rated input power | 10mW |
Maximum input power | 100mW |
Microphone Specification | |
Type | Transducer Moving coil dynamic MIC |
Sensitivity Range | -60± 3dB |
Impedance Max | 150Ω at 1kHz |
Frequency | 500-6KHz |
Can you please advice can we use this with the same circuit diag shown in above post.
Regards
Akash Jain