Other Parts Discussed in Thread: TPA3129D2, TPA3110D2
Hi.
I am trying to develop an Audio Power AMP up to 30W in Mono Mode.
I want to use one 8Ω speaker at 12V.
The TPA3128D2 and TPA3129D2 are under review.
According to the datasheet, the TPA3128D2 can be connected in PBTL mode enabling up to 60W output power. Would it become about 30W output power at 12V?
The TPA3129D2 just mentions Mono Mode, not PBTL Mode. Isn't PBTL Mode supported? Is it possible to output maximum 30W when in Mono Mode?
Similar to the TPA3128D2, the TPA3110D2 uses OUTPL / OUTNL and OUTPR / OUTNR in PBTL mode configuration. Since it is a 2x15W AMP, can the TPA3110D2 operate up to 30W at 24V input?
Thanks.