Hi!
I am designing a system where I would like to be able switch between driving a 32 ohm headset and outputting an attenuated signal that can drive a microphone input (using an L pad)
What is the state of these outputs when they are not powered? Are they high impedance when they are not powered. I was thinking of combining the output into 1 audio jack and if the pins are high impedance when they are not active, I will be able to combine the line outputs and headset outputs without any external analog muxes.
Best regards,
Stefan