I made a PurePath build of a parametric equalizer. It was initially set at 44.1K sample rate. I need to change to a 48K sample rate to support other parts of my hardware. I made the change in PurePath, ran the build but do not see a change in my performance. My center frequencies are skewed. I see this in the system Setting Code and it appears that there are no differences for between 44.1 and 48K.
%%if (%%prop(SampleRate) == 44100 || %%prop(SampleRate) == 48000)
reg[0][0][7] = 0x08 ; P=1, R=1, J=8
reg[0][0][13] = 0x00 ; DOSR = 128 (MSB)
reg[0][0][14] = 0x80 ; DOSR = 128 (LSB)
reg[0][0][18] = 0x02 ; NADC Powerdown NADC = 2
reg[0][0][19] = 0x90 ; MADC Powerup MADC = 16
reg[0][0][20] = 0x40 ; AOSR = 64
%%endif
How do I change to 48K?
Joe