Hi,
For my application I need the left channel fully differential output and the right channel single ended output. Both using the high power driver and AC coupled.. Is it possible to accomplish with this device?
In register 14, bit D6 select differential mode for both output stereo, bit D7 select AC-coupled mode for both output stereo. It is all or nothing
In register 37 and 38, we can select also differential mode by choosing what to do with HPxCOM output. Here, the left and right side are independent.
It seems to me, there are overlapping settings between registers.
What if I configure the device as follow: Reg 14=0xC0, Reg 37= 0xC0, Reg 38=0x0C ? Am I going to have the correct level, since on the right side, I use only HPROUT pin.
Can you explain what the following bit are really doing in the device: register 14 bit 7,6, 3
Thanks