I am using the PCM1792A and noticed some unwanted behaviour.
1) The DAC is running (48kHz, 3,072MHz, 12,288MHz or 24,576MHz). The output has HF Noise on it, even when sending nulldata over the PCM interface. When I stop the clocks, the output is clean. I've measured the clocks and their phase but they look good. What could cause this HF noise on the output?
2) I've also seen dips every Fs/8 in the output if B4 in Register 20 (DFTH) is set. Is this normal?
The DAC is configured as follows:
B6 in Register 20 (SRST), 300us delay, B4 and B5 in Register 18 (FMT0 and FMT1, 24 bit Left Justified).
My schematic: