Hello Guys,
Good day.
We have a customer who wants to confirm the following:
1) Is it okay to leave one channel of the PGA2310 unconnected when only one is used? Or will it cause any problems?
2) Can I used the remaining unused channel for another signal, for example from an microphone?
3) When two PGA2310 are daisy chained together, will the data which is meant for the last IC in the chain, cause any change on the first IC of the chain? Or will the first IC just pass the data to the second IC?
Thanks to confirm!
Art