Part Number: TLV320DAC3100
hello
I have some questions similar as below.
https://e2e.ti.com/support/audio/f/6/t/833136?tisearch=e2e-sitesearch&keymatch=TLV320DAC3100
input clk/pwr to TLV320
MCLK 12Mhz
DVDD 1.8V
IOVDD 3.3V
AVDD 3.3V
SPVDD 5.0V
Circuits on SPKP/SPKM lines(Refer to TI application report SLAA581)
Series Bead(120 Ohm-100Mhz, 50m Ohm DCR) and parallel capacitor(470pF), respectively.
TLV320 registers configuration
/cfs-file/__key/communityserver-discussions-components-files/6/4760.Audio_5F00_LP1_5F00_Register.txt
When speaker(8 Ohm) is working, I measured some waveforms as followings
Fig#1 SPKM(Speakerout-) overshoot voltage and ring voltage
Fig#2 SPKM(Speakerout-) ring current
My questions are
1. regarding Fig#1, if the overshoot(about 1.7V) will cause damage to TLV320?
2. regarding Fig#1 and Fig#2, are the ring voltage and ring current normal?
3. I have observed that no matter what sound is played, the frequency of SPKM/SPKP output remains around 300KHz, is it normal?
Thanks and best regards
TC Liu