Part Number: TAS5805M
Hi.
I was playing a little bit with the different Process Flows available for the TAS5805M in PBTL mono mode.
When using (1.0 48k) it is supposed than it hasn't fs auto-detection, but as there is no place in the Tuning and Audio Processing to set the fs and BCK audio, I tried to play 44.1kHz audio leaving SIG_CH_CTRL Register (0x28) in 0x00 (auto detection mode)
The audio was played without problem during a while, but after some time a CH1_OC_I fault rise in the CHAN_FAULT Control Port Register (0x70)
If I cleared the fault, I could play audio again till the fault rise another time.
If I set manually the fs (44.1kHz) and the BCK ratio (32·fs) writing 0x38 in the SIG_CH_CTRL Register (0x28), the OC fault never occurs.
I understand that I should set manually the fs and BCK ratio when using (1.0 48k) Process Flow as it is stated it hasn't auto-detection, but what I can't understand is why it can work for a while and after a time it rises an over current error. I expected a clock error related fault, not an over current one. Why is this?
Regards,
Juan Pablo Novo