Dear Sirs,
While my customer did the short mode protection function of output , they found there is some different with datasheet.
The protection mode that customer use is CB3C and they found there are 2 kinds of test result that shown as below waveform.
Ch1: OCP signal, Ch2: current waveform for OCP, CH3: input sine wave, CH4:TPA3251 output current
Result 1:
Result 2:
Note:
1. CH1 and CH2 are waveform by customer protection design
2. As waveform we can see, CH2 waveform will change related with different TPA3251 output current
3. TPA3251 output inductor is 44uH, and output cap is 1uF
4. input waveform is 60Hz sine wave
5. customer hope the output is always result 2.
Please help to advice:
1. What reason will cause the result 1 happen?
2. Is there any design modification suggest?
Thanks.