Other Parts Discussed in Thread: TAS6424
I used a dsp to control and transmit audio to tas6422 .but the warn pin was pulled lower .so I want to write data control to the register through i2c but tas6422 did not respond. The response signal is high level. I have checked the circuit related voltage voltage is normal pvdd And vbat voltage is 12v vdd is 3.3v i2c pull-up resistance is 4.7k ohm .Is this chip broken?Is the driver wrong? But I use this program to control the gyroscope can indeed communicate normally.I feel so confused!