Other Parts Discussed in Thread: PCM5242, DAC11001A
Hi,
I use Spartan-6 as a master, so I am going to program DAC without using the PurePath Console (if that's possible). I am going to use PCM5252 to generate a sinusoidal 150 Hz (I am working with biosensors application, that's why 32-bit resolution is crucial for me to achieve minimum voltage resolution steps)
I would like to know in which order I should write the pages and registers (page 0: reg 1 - 125; page 1: reg 1 - 9; page 44: reg 1; page 263: reg 63-64)? I didn't find the exact writing registers sequence instruction in the datasheet.
Thank you in advance,
Roman.