Datasheet shows a 1.5KOhm pull up on _FAULT pin.
What is the min-max Rpu values supported on this pin? What is the typ/max current of this open drain output?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Datasheet shows a 1.5KOhm pull up on _FAULT pin.
What is the min-max Rpu values supported on this pin? What is the typ/max current of this open drain output?
Hi, Eddie,
Sorry for the late response.
As mentioned in the datasheet ( 7.3.5 Open FAULT Output ), the pull-up resistor should be at least 1.5Kohms. There's no restriction for a higher resistor.
Regarding the open drain output current, the typical value is 3mA. There could be a max variation of 1mA.
Best regards,
Luis Fernando Rodríguez S.