Hi
We have selected TPA3111D1 in one of our projects, for driving 8 ohms, 1 Watt speaker.
While simulating the circuit in TiNA, i have observed that at higher gains, when the output gets saturated, the input signal also is getting distorted. Please see the below waveform capture. Could you please share your thoughts on this.?
"Vin to IC" is the signal probed at positive input of the amplifier. I have a piece-wise linear signal as the input, which is low pass filtered and ac coupled to the amplifier
At lower gains of 20dB and 26dB, the input and output are sinusoidal.