Other Parts Discussed in Thread: INA592
Hi sir,
For the item of "differential voltage range" is "see serial curve" in datasheet, but because the table is not found, can you tell the differential input voltage range?
Also, the "common mode voltage range" "3(V–)+3~3(V+)–6" exceed power supply voltage,
Can I use Differential Voltage Range in the same case of beyond power supply voltage?
e.g. Is it possible to get output of 11Vp-p base upon the condition below?
-power supply ±10V
-G=1/2
-differential signal input +20dBu( 22Vp-p:+IN 11Vp-p, -IN 11Vp-p)
I think it's possible to use it in the same way due to INA137 is similar to INA592.
is it correct?
Thanks.
Regards,
M