I was wondering if it is possible to query static and live internal quantities of the TAS2563; for example, the currently loaded tuning parameters (e.g. T/S parameters, EQ setting, etc.), as well as current temperature, battery, etc. By live quantities, I mean the ability to obtain information such as an impedance curve that is not the one that is stored in the model, but the actual ability to measure the impedance vs. frequency of the current speaker being tested.