Part Number: TAS2563YBGEVM-DC
Other Parts Discussed in Thread: TAS2563
Hi Sirs,
With the same TAS2563 CFG of 0x98+0x9A and 0x9C+0x9E. The TAS2563 EVM works with slve addresses of 0x98 and 0x9A, but no sound with 0x9C+0x9E.
The TAS2563 devices can send ACK with the 0x9C and 0x9E, Class-D PWM is running but no sound.
Would you pls review the encosed CFGs to provide tips to bring up the TAS2563 with 0x9C and 0x9E?
We generated 0x9C and 0x9E codes with PPC3 GUI:
0x98 + 0x9A Hardware Setup - Ext I2S ASI. I2C ACK + Class-D amp works normally
Class-D PWM waveforms - Sounds normally
0x9C + 0x9E Hardware Setup: - Ext I2S ASI. I2C ACK, Class-D PWM is running but no sound 
Class-D PWM waveform - No sound
Thank you and Best regards,
Wayne Chen
09/15/2020
0x98+0x9A CFG
TAS2563_Stereo_Test_0x98_0x9a_48KHz_EC_BIN1_Fullset.cfg
0x9C+0x9E CFG
TAS2563_Stereo_Test_0x9c_0x9e_48KHz_EC_BIN1_Fullset.cfg