hello,
can PCM 9211 accepts direct HDMI ARC 1.4 output from my TV?
Using pin no 19 and 14 as HEAC+ and HEAC-
If yes can i convert it to analog stereo audio signal?
Anyone worked on this type of project?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
can PCM 9211 accepts direct HDMI ARC 1.4 output from my TV?
Using pin no 19 and 14 as HEAC+ and HEAC-
If yes can i convert it to analog stereo audio signal?
Anyone worked on this type of project?
Hi,
The PCM9211 can accept HDMI ARC 1.4, but NOT eARC. The inputs to PCM9211 are only single-ended though so you would only use the HEAC+ pin and the device is really designed for 2 channels of data so if you are trying to convert to I2S there will be some limitations. The device can output an S/PDIF signal on the MPO pins, but it cannot convert to an analog stereo signal that you might use to drive a speaker or such.
Best,
Zak
Hi Nitin,
I2C is only used for configuration, audio data is transmitted over I2S. HDMI ARC is formatted very similarly to S/PDIF, so you should be able to translate this to an I2S output using the PCM9211, keeping in mind that the PCM9211 only supports 2 channels of audio over I2S. You could then feed that signal to a digital input, analog output class D audio amp.
Best,
Zak