This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM9211: DSD

Part Number: PCM9211

Hi team,

Figure 36 on page 53 of PCM9211 datasheet describes the output of DSD from main port

1) Can DSD signal be input from MPIO_C port and output from MPIO_B port?

2) The clock signal of DSD shown in Fig. 36 passes through DIT. Input DSD signal from MPIO_C port. If MPO0 or MPO1 is turned on, can coaxial audio signal also be output?

  • Hi Amy,

    From the datasheet I do not believe that MPIO_B can serve as a DSD output port and unfortunately I do not have a DSD source to try and test this. It looks to me like the DSD signal is only used to feed back to the DIR to generate a cleaner version of SCLK. You could enable the MPO paths, but I don't think you will see valid audio data out.

    Best,

    Zak