Part Number: TAS5411-Q1
Hi,
I am working on automotive project with below p/n:
Codec: TLV320AIC3109-Q1
Amp class D: TAS5411-Q1 8-W
The codec is connected to an embedded system with modem (based on Linux system) via I2c (controls) and via Audio serial data bus (data).
I need the Linux driver because I have to integrate it into the embedded system.
I did not find anything in ti.com
I don't know if there is also a linux driver for the amplifier.
Do you know where I can find this information for TAS5411-Q1? For the codec I already have them.
Thank You,
Antonio