This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PCM1840: Can I select which analog inputs are used in I2S mode?

Prodigy 20 points

Replies: 2

Views: 50

Part Number: PCM1840

Hi!

Can I select which inputs are used in I2S mode?

For example I want to use channels 2 and 3 /check attached picture/

  • Hi Daniel,

    In 2-channel modes the device uses channels 1 and 2. To see channels 3 and 4 the device must be configured for 4-channel TDM.

    Best,

    Zak

    Regards,

    Zak Kaye
    Precision Data Converter Applications

  • In reply to Zak Kaye:

    Hi Zak,


    I understand.

    Thanks for the fast response.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.