This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1840: HPF cut off frequency

Part Number: PCM1840
Other Parts Discussed in Thread: TLV320ADC6140

any chance to lower the HPF cut off of PCM1840 or to switch off the HPF? 24Hz @96KHz and 48Hz @192KHz hurts within high-end audio amps! 

  • Hi Hanno,

    The HPF for PCM1840 is fixed at 0.00025*fs and since this is a HW controlled device with small area it unfortunately is not configurable. If you need similar performance with the option to program this I would suggest TLV320ADC6140.

    Best,

    Zak