This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 113
Part Number: TLV320DAC3203
Hi!
We are looking at cross reference requirements for the AK4370 for both commercial and automotive applications. What 2-channel DAC with integrated headphone driver can TI recommend as a replacement or upgrade?
AK4370 is replaceable with TLV320DAC3203 because it has an integrated headphone amplifier capable of delivering 45mW into 16Ω, supports sample rates up to 192kHz, can operate from a 1.8V or 3.3V supply, and comes in a 24-pin QFN package.
AK4370 is replaceable with TLV320DAC32 because it has an integrated headphone amplifier capable of delivering 50mW into 16Ω, supports sample rates up to 96kHz, can operate from a 3.3V supply and comes in a 32-pin QFN package.
The TLV320DAC3203 documentation can be downloaded from the links below:
For additional information about the TLV320DAC3203, please take a look at the product folder:
https://www.ti.com/product/TLV320DAC3203
The TLV320DAC32 documentation can be downloaded from the links below:
For additional information about the TLV320DAC32, please take a look at the product folder:
https://www.ti.com/product/TLV320DAC32
More info on Excel sheet:
1581.TLV320DAC3xxx_parameter_data.xlsx
I hope this helps!
Best regards, Luis Fernando Rodríguez S.