This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PCM3060: AK4621 Replacement and Upgrade Options

Expert 8930 points

Replies: 1

Views: 106

Part Number: PCM3060

Hello,

We are looking at cross reference requirements for the AK4621 for both commercial and automotive applications. What CODEC can TI recommend as a replacement or upgrade?

Regards,

Aaron

  • The PCM3060 is a stereo audio CODEC that includes a 99dB SNR ADC and a 105dB SNR DAC and would make a good replacement for AK4621.

    The PCM3070 can serve as an enhanced version of the PCM3060. The PCM3070 is a stereo audio CODEC with slightly lessened performance but has more audio processing capability with an integrated programmable miniDSP.

    Since there are no automotive qualified versions of the PCM3060 or PCM3070, the TLV320AIC3254-Q1 can be a good substitute. The TLV320AIC3254-Q1 is a stereo CODEC that offers multiple inputs/input muxing capabilities , max sampling rate of 192kHz and an integrated programmable miniDSP.

    Regards,

    Aaron

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.