This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 169
Part Number: PCM3168A
Hello,
We are looking at cross reference requirements for the AK4628 for both commercial and automotive applications. What CODEC can TI recommend as a replacement or upgrade?
Regards,
Aaron Estrada
The PCM3168A and the PCM3168A-Q1 are commercial and automotive, multi-channel CODECs that are a great replacement option for AK4628. The PCM3168A is the only multi-channel CODEC available with a 6-channel, 107dB SNR ADC and an 8-channel, 112dB SNR DAC.
The PCM3168A also offers an ADC sampling rate range of 8kHz – 48kHz and a DAC sampling rate range of 8kHz – 192kHz.