Hello,
I open a related question to the thread with the same name (e2e.ti.com/.../942769 because I could not reply directly in the initial thread.
In order to understand what I will explain and ask after, I suggest that you read the previous thread (the link is given above).
Following our previous discussion, we have changed the threshold for the tests we made in order to take into account the gain error impact on the Dout amplitude values measured.
However we have recently seen that even with this adjustment some of our equipments have an amplitude higher than the new threshold fixed.
My goal is now to find a way to put more controlled thresholds on the Dout value measured.
I have made some more tests where I send a sine wave at 1kHz and only change the Volume_In and Volume_Out parameters. The values measured are :
- The AC tension in the hard loopback
- The Dout amplitude value
The values measured on two equipments are given below :
Volume_In | Volume_Out | Digital Amplitude Dout1 | Digital amplitude Dout2 | Loopback tension 1 | Loopback tension 2 |
25 | 80 | 2482 | 2593 | 46mV | 48mV |
40 | 80 | 9520 | 9928 | 65mV | 65mV |
45 | 80 | 14448 | 14897 | 68mV | 67mV |
50 | 80 | 21336 | 22203 | 73mV | 74mV |
60 | 80 | 45951 | 47696 | 80mV | 80mV |
75 | 80 | 65535 | 65535 | 87mV | 87mV |
100 | 80 | 65535 | 65535 | 94mV | 95mV |
25 | 100 | 7834 | 8179 | 80mV | 81mV |
100 | 100 | 65535 | 65535 | 180mV | 185mV |
75 | 75 | 65535 | 65535 | 78mV | 77mV |
As you can see, the AC tension is almost the same between the two equipments but there is a gap on the digital amplitude measured.
For example, for a Volume_In of 25 and a Volume_Out of 80, we have changed the threshold from 1980 < Dout < 2520 to 2100 < Dout < 2600. But on some equipments we recently measured a Dout value of 2680.
I know that we can change the thresholds again according to the biggest value we measure today but nothing can insure us that even with a new change we will not measure a higher value again.
According to the highest value of the ADC gain error (1.2dB mentioned on the previous thread), is there a way to define thresholds based on this value and on the AC value measured ?
Thank you again for your help.
Matteo