Dear TI team
I would like to ask about PCM1794A.
Our customer is considering using the PCM1794A in DF-Bypass mode.
I would like you to tell me about the following.
1.Our customers are trying to use with the following settings
(Sampling cycle is 128kHz)
・ SCK: 32.768MHz
・ BCK: 8.192MHz
・ WDCK: 128kHz
The above frequencies were not mentioned in the data sheet, but is there any problem with the above settings?
(Is it possible to use the above frequencies by calculating from the External Digital Filter Application Timing Requirements in the data sheet?)
2.Regarding DF Bypass mode, I checked the data sheet to see what the output waveform would look like, but there was no reference measurement waveform.
Is there any data of the output waveform in DF Bypass mode?
(I want to know whether it is output at a constant voltage or oscillated at a certain frequency.)
Best Regards,
Y.Ottey