Other Parts Discussed in Thread: TAS2558
Hi Sirs,
According to the TAS2557 datasheet, it support sample rate up to 96kHz. However, there is no 96kHz option with PPC3 GUI.
Would you please provide tips to bring it up to 96kHz SR? We tried to configure it by PPC3 GUI, but it was in vein.
TAS2558 datasheet:
Sample rate option on Book 0x00, Page 0x00, Register 0x2F
PPC3 default 0x2F=0x2A -> It works with 48kHz sample rate:
Wrote 0x2F = 0x2B -> OK with 12.288MHz MCLK, 96kHz LRCK
Wrote 0x2F = 0x2B -> No sound with 12.288MHz MCLK, 96kHz LRCK
The TAS2557 EVM works with 96kHz, 24.576MHz MCLK in ROM mode 1 and ROM mode 2. Does it mean that the TAS2557 an support 96kHz in ROM mode only?
OK with 96kHz SR, 24.576MHz MCLK
Distorted with 96kHz SR, 12.288MHz.
Thank you and Best regards,
Wayne Chen
11/20/2020