Hello,
My customer has several questions about the test result of TAS2505.
The customer measured TAS2505 using the evaluation board, and with CM=0.9V, Speaker Amplifier Volume +12dB and SPKVDD = 5V, voltage of SPKP and PPKM was 2.5V. From this result, they estimated that the offset of the speaker amplifier in the output stage is 1/2 of SPK VDD. Is it correct?
If it is correct, the customer also wants to ask these farther questions:
- What is the variation accuracy of 1/2 offset voltage? (Accuracy when generating 1/2 from SPK VDD)
- The relationship between CM = 0.9V and the above-mentioned 1/2 voltage. Where in the circuit are those voltages switching?
I'm looking forward for your reply.
Best Regards,
Ryotaro Fukui