Part Number: PCM3060
Hello,
Regarding to BCK1/2 high/low time on PCM3060,my customer is asking a question.
(Question)
According to datasheet Figure24, BCK1/2 high/low time is described as following.
Why do these times have range from 40% to 60%? Why isn’t these fixed to 50%?
They think BCK is divided by SCKI. At that time, BCK and SCKI are even ratios of integers.
So, the duty ratio should be fixed to 50%.
Could you please tell us why these times have range from 40% to 60%?
(My customer configuration)
・LRCK=1fs
・BCK=64fs
・SCKI=512fs
(BCK= 1/8 * SCKI)
*In above case, will the duty ratio be fixed to 50%?
Regards,
Tao_2199