This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 58
Part Number: PCM3060
Dear TI
I would like to know the ESD (MM/HBM/CDM) rating of PCM3060.
A customer of mine is asking for the ESD ratings so that they can protect against harming the part during handling and loading on PCB. Please advise.
Best regards.Ohkuma
Hello Ohkuma,
I have reviewed our internal databases and found that the PCM3060 was very thoroughly tested for ESD and will meet the following ratings:
MM: 200V
HBM: 2000V
CDM: 1000V
Note that I have made this thread an FAQ thread since it is a common question and will likely come up again.
Regards,Collin WellsPrecision ADC Applications