In the datasheet, the input resistance is only given for analog inputs routed to ADC input. When the input is in analog bypass mode, it is routed to an output mixer instead.
What is the input resistance on LINE2R, LINE 2L in differential and analog bypass modes when routed to HPROUT/HPLOUT through a mixer?
Here is the codec configuration:
Reg 20=0xF8 : Line 2L is not connected to ADC
Reg 23=0xF8 : Line 2R is not connected to ADC
Reg 37=0xC0 : Both DAC powered up, HPLCOM differential
Reg 38=0x04 : HPRCOM differential
Reg 40= 0xBC : output CM=1.65V, Line2L/R enabled in differential bypass mode, soft stepping 1 per fs
Reg 41=0x00 : Left DAC uses DAC_L1 path, Right DAC uses DAC_R1
Reg 45= 0x80 : Line2L routed to HPLOUT, 0 dB attenuation
Reg 62= 0x80 : Line2R routed to HPROUT, 0 dB attenuation
Reg 82=0x80 : DAC_L1 routed to LEFT_LOP/M , 0 dB attenuation
Reg 92=0x80 : DAC_R1 routed to LEFT_ROP/M , 0 dB attenuation