Part Number: TAS5782M
Hallo
We are using the smart amp feature of the TAS5782 amplifier. I have made a Klippel Measurement of our woofer to get the speaker parameters which are required to put in the smart amp. I have attached the text file with the TS parameters of the driver. Also a PPC3 file, where I have input the data in the woofer characterization page. But when I look at the final data the Vas value seems to have changed after entering all the values. My original Vas value was 0.218 L but after entering all the values the Vas value in PPC3 changed to 0.000218 L. Any explanation what went wrong or why this is happening. All the other parameters look fine.
When Using the Smart Amp and learning board it is possible to measure the SPL response of the driver and load it in the characterization file, would it be possible to load the SPL data also if we do the SPL measurement using a external microphone not the leaning board.
On the Smart Bass there is a parameter called Xmax, which is the maximum excursion, but is it the peak value or the rms value?
thanks in advance