This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV1012 - What is the Drive capability ?

Other Parts Discussed in Thread: ADS803, LMV1012

Hi,

I am using a MEMS Microphone ADMP504 whose output is to be fed to a 12 bit ADC.

ADC i have chose is ADS803.

This ADC has an input capacitance of 20pF (Typical).

Since the MIC's output is only 0.25V peak-peak, i am using LMV1012 pre-amp at the MIC's output.

I am not sure whether this LMV1012 pre-amp can drive the ADC.

I could not find load drive or output capacitance data mentioned in the LMV1012 datasheet.

Could you please help me on this ?

Below is my MIC + Preamp Ckt.

Thanks and regards,

Karthik