Hi,
I am using the LM3886 chips for an active speaker with logic operated mute control.
Two LM3886 chips are used in each speaker, and I need to mute/unmute both chips simultaneously. I would like to connect the mute pins (pin 8) of each of the two chips, in order to control them using one common MOSFET switch (with a series resistor on its low side) instead of two. I have simulated a muting circuit drawing 1 mA through a common MOSFET switch when in unmuted mode (theoretically 0.5 mA from each chip). As I do not know exactly how the internal circuitry of the chip looks like, I am not able to predict the impact of doing this. I am afraid this solution may not guarantee an equal repartition of the two currents, ending up with one chip muted and the other not. For all I know, a such connection between two chips may cause crosstalk related problems as well.
Can anyone tell me if this solution is reliable, or if I rather should use separate switching devices for each chip? Can I rely on pin 8 having a potential of -2.6 V?
Best regards,
Torje