Other Parts Discussed in Thread: TPA3110D2
Hi,
I'm doing tests with a sound card that drives two speakers by BTL 8 ohm 2 watt and I saw doing the math by using an input of the TPA3110 1 volt peak to peak , 24V power supply, I must have a maximum gain of 27dB, but sometimes I have ,with setting 26db gain, fault signal go low and the audio is turned off, I have to limit the output with the PBTL? (Not used)
Can I use the same speakers in parallel ( 4 ohm having the same power 2W ) with the 24 V?
Can I connect speakers of the same type with a cable length of 10 meters? I must use a shielded wire with particular size ?
Best regards